Your questions answered: Critical power: Emergency power

The May 4 “Critical power: Emergency power” Webcast presenters addressed questions not covered during the live event.

Share This Article


Electrical engineers must consider many factors when designing emergency power systems. Safety, maintainability, code compliance, and economics play crucial roles in determining the topology of an emergency system for a critical facility. Specific requirements for emergency power vary based on building occupancy type, facility use, and critical function.

When designing generator systems, engineers must ensure that the generators and the building electrical systems that they support are appropriate for the specific application. They must make decisions regarding generator sizing, load types, whether generators should be paralleled, fuel storage, switching scenarios, and many other criteria. Emergency power systems provide power to ensure that life safety systems and critical equipment can operate during a power outage. NFPA 70: National Electrical Code (NEC) Article 700: Emergency Systems defines the category that applies to emergency generator power sources.

The May 4, 2017, “Critical power: Emergency power” Webcast presenters addressed questions not covered during the live event. The experts are:


  • Tom Divine
    PE
    Senior Electrical Engineer,
    Smith Seckman Reid Inc., Houston
 

  • Freddy Padilla
    PE, ATD, Principal
    MEP Engineering Director
    Austin, Texas
 

Question: Are fire pumps required to meet the requirements of NFPA 70-2017: National Electrical Code (NEC) Article 700, in addition to Article 695?

Freddy Padilla: Fire pumps are not required to meet Article 700. The key point about fire pumps is that you should always check with your authority having jurisdiction (AHJ) to ensure that your source or sources are per NEC Article 695.3. But these sources are not required to comply with Article 700.

Q: Why does NFPA 110-2016: Standard for Emergency and Standby Power Systems allow natural gas generators, but NEC Article 700 requires an AHJ exception?

Tom Divine: NFPA 110, 2016 edition, Paragraph 5.1.1(3) allows natural or synthetic gas as a fuel source for generating systems. The exception to 5.1.1 requires onsite fuel storage, with automatic transfer to the onsite supply, for Level 1 systems where the probability of fuel delivery interruption is high. A Level 1 system is one whose failure could result in the death or serious injury of a human. In this context, a high probability would be, in fact, a small chance of interruption.

In the 2017 edition of the NEC, Paragraph 700.12(B)(3), prohibits the generator for an emergency system from relying strictly on a public utility system for its fuel supply. The exception allows an AHJ to determine or assess the likelihood that the utility electrical supply and the offsite fuel delivery system will fail simultaneously, and, if that probability is, low, to permit the use of other than onsite fuels to serve the prime mover.

In practice, these requirements are quite similar: both require onsite fuel storage, unless a determination has been made that offsite fuel delivery is reliable enough to be acceptable to the AHJ as the sole source of fuel for the alternate source.

Q: How can we classify mission critical projects, if we are not required to have coordination protection?

Padilla: The reliability of mission critical project is not regulated by the AHJ or the NEC. Selective breaker coordination is a requirement that needs to be discuss with your owner. There are several standards that recommend breaker coordination, such as Uptime Institute and TIA-942-A. Remember, unless requested by you (owner), these are only recommendation or good practices, not a requirement of the AHJ.

Q: Please list some sample buildings that are typically designated for critical operations power systems (COPS).

Divine: The original draft of proposed NEC Article 585, which later became Article 708 in the 2008 NEC, carried a fine print note (FPN) with a fairly extensive list of candidate facilities. That FPN was deleted from the final version, ostensibly out of concern that it would be interpreted as a requirement that all such facilities be classified as critical operations areas requiring a COPS. Under Article 708, the NEC describes installation requirements for a COPS, but doesn’t determine when a COPS is required. That determination is left to other codes, statutes, or determination by a governmental authority. Here’s the list of candidate facilities from the draft of Article 585:

 

  • Air traffic control centers
  • Central station service facilities (fire and security system monitoring)
  • Chemical, petrochemical, and hazardous material (including biohazard) handling facilities
  • Communications centers, telephone exchanges, and cellular tower sites
  • Emergency evacuation centers
  • Financial, banking, and business data processing facilities
  • Fuel supply pumping stations (i.e., natural gas distribution and delivery infrastructure)
  • Hospitals and associated support facilities
  • Municipal infrastructure: water and sewer treatment facilities, 911 centers, and offices and facilities deemed critical to continuity of government
  • Police, fire, and civil defense facilities including power for radio repeater operations
  • Radio and television stations
  • Transportation infrastructure: airports, rail stations, and seaports.

 

Q: Should a generator-mounted circuit breaker be directly connected to the same size main breaker within a building? Do these two breakers need to be selectively coordinated because the operation of either breaker will result in the same outage?

Padilla: No, these two breakers are in series. See exemption in NEC-2017 Article 700.32.

Q: Can you install the emergency generator and the automatic transfer switch in the same room?


Divine:
NFPA 110, 2016 edition, Paragraph 7.2.1, calls for the emergency power supply (EPS), which covers the generator(s), to be installed in a separate room for a Level 1 system. Paragraph 7.2.1.2, though, specifically allows installation of components of the emergency power supply system (EPSS), which includes transfer switches, in the room with the EPS. A Level 1 system is a system whose failure could result in loss of life or serious injury to humans. In the 2010 edition, currently enforced by the Centers for Medicare and Medicaid Services for health care facilities, that permission appears in Paragraph 7.2.1.

Q: Are fire pumps legally required standby loads?

Padilla: No, fire pumps are not legally required load. Fire pump services don’t need to comply with NEC 701.

Q: What is the level of selective coordination required for an NEC Article 700.27 system?

Divine: Presuming that the reference is to the 2011 edition of the NEC, Article 700.27 requires that emergency system overcurrent devices be “selectively coordinated with all supply side” devices. Selective coordination is defined in the 2011 edition as, “localization of an overcurrent condition to restrict outages to the circuit or equipment affected, accomplished by the choice of overcurrent protective devices and their ratings or settings.” No specific level of coordination is specified, leaving the interpretation to the AHJ. Some enforced the requirement quite strictly, while others allowed for a measure of compromise between selectivity and other objectives.

The definition in the 2017 edition is more restrictive, adding the text, “… for the full range of available overcurrents, from overload to the maximum available fault current, and for the full range of overcurrent protective device opening times associated with those overcurrents.” That language is generally interpreted as not allowing for any failure of selectivity under any circumstances—a very demanding requirement.

Q: In a COPS facility, is ground fault trip required on the generator and feeders, or is ground fault indication as in health care facilities acceptable?

Padilla: If your generator also is used to serve emergency loads, you can take that to eliminate your ground fault protection, but if you are not using the generator for emergency load, you might need to provided ground fault protection. A good option to avoid this requirement is to provide a high resistance ground and your ground fault protection is not required. See NEC Articles 230.95 and 250.36. Also, you can call for an Article 230.96 exception if this applies to your building type.

View the original article and related content on Consulting Specifying Engineer