Throughout the year, inclement weather can threaten the stability of the power grid. Power outages threaten an organization’s data, employee safety and customer loyalty. One way to mitigate those risks is with a backup generator. During hurricane season, ensuring reliable generator operation means routine maintenance. Maintenance can be performed by your own trained technicians or as part of a maintenance contract with your Generac Industrial Power dealer. Fuel Reliability If yours is a diesel-fueled generator — and unless you’ve experienced power outages so frequent and severe as to quickly consume an entire tank of fuel — the beginning of the new year is an excellent time to perform fuel maintenance. Diesel fuel tends to degrade over time and will require filtering and polishing to eliminate moisture and contaminants that, if introduced to the engine, could at a minimum reduce performance but run a real risk of causing engine damage. Inspecting Spark Plugs While gaseous-fueled generators have the benefit of operating on a fuel that is largely unaffected by extreme weather, one thing that can impede successful gaseous-fueled generator operation is bad spark plugs. Pitted and fouled spark plugs could cause the engine to misfire repeatedly or fail to start entirely. To avoid increased exhaust emissions and improve the generator’s ability to start, the spark plugs should be inspected — and changed, if necessary. The Engine’s Electrical System Generators can only produce power if they receive power — in the form of DC voltage coming from the starting batteries. Dead batteries mean a dead generator set. Batteries run the risk of losing their charge over time. They should be inspected for damage, and a load tester can help determine if the battery is having difficulty maintaining a charge. Make sure battery fluid levels are properly maintained, and ensure that cables are securely fastened to the terminals and that both are clean. Changing Engine Coolant Coolant prevents the development of rust deposits, keeps the generator’s water pump well-lubricated and helps remove contaminants from the gen-set’s system. Maintaining engine coolant keeps the generator prepared for harsh weather and helps ensure its long-term performance. The coolant should be flushed and changed at least once per year or after every 100 hours of operation — whichever comes first. Inspecting And Changing Filters Dust, dirt and debris can invade your generator. Luckily, oil and air filters are designed to serve as the engine’s first line of defense against these harmful contaminants. The generator’s oil filter — or filters — should be changed at least once per year to keep debris out of the engine and prevent potential damage. The beginning of the new year is an excellent time to change the oil and filter. Load Bank Testing While a generator may start flawlessly, there’s no way of knowing if it’s actually producing the power it should unless it is periodically connected to a load bank. Load banks allow the generator to run under load in a simulated outage situation. They test the generator to see if it will perform as intended during a real power outage. Load bank testing should be performed annually.