News & Events
Loading...
How to Choose the Right Standby Generator 10/7/2009

Waukesha, Wis. – October 7, 2009 – Choosing the right standby generator for your home is just like selecting a new dishwasher or refrigerator – you have certain needs and you want the best. Generac® Power Systems, Inc. has recognized the need to educate the public and make it easier to make the right decision when choosing the appropriate generator for the home.

There are a number of items to consider when deciding what back-up power solution will work best for one’s home and lifestyle. It is important to do the research and read between the lines – especially when a family’s safety is at risk.

Generac has developed this easy guide for consideration as you begin the process of purchasing your new standby generator.

1)         Who makes it? – Be aware of the company’s reputation and leadership in the generator category. It helps to choose a brand that is solely focused on generators to ensure you are getting a quality product from a trusted company.

2)         Exterior Shell – Don’t overlook the exterior shell of the generator! Be sure the external enclosure, or casing, of the generator has easy access for servicing. Hinged enclosures are best. Be sure to stay away from bolted enclosures which make it much harder to service the generator. Also, be sure to choose a generator with a rust-resistant shell, ensuring longer life of the generator.

3)         Sound Levels –Be sure to consider the sound decibel of the generator to ensure your generator won’t wake your family at night or interrupt your favorite television program. Most reputable standby generators will sound similar to an air conditioning compressor…or even quieter.  Look for models that feature a quiet mode during its weekly self-test, when most home owners will hear their generator running, since actual power outages are less frequent.

4)         Engine Basics/Sizing – Just like a car, the generator’s engine is its heart.  Smaller size generators use air-cooled engines while larger ones use liquid-cooled engines with separate cooling systems. 


In either case, look for engines built for heavy-duty generator usage, and not adapted from other products.  The better engines have longer service intervals, requiring oil changes after every 200 hours of service or even longer. Beware of the electrical load your generator says it can handle. Do your math! Be sure the power of the generator matches the power needed to back up the circuits and appliances in the home you want to back up. Customizable solutions should always be an option. 

5)         Day-to-Day Operation/Ease of Use – The generator should have its own programmable controller to allow for hands-free operation and is another key element to examine before purchasing a generator. The controller should act as the brain of the generator and alert the homeowner when it is in need of maintenance – making the generator very user-friendly for the busy homeowner. The best generators on the market today are much more homeowner-friendly and should work just like a normal kitchen appliance.  They have control panels that communicate with plain language that is visible on a LCD display, not just a series of warning lights.

6)         Warranty – Keep your eye out for warranty offerings and additional seals of approval – these are important. A quality generator company will always offer warranty flexibility that fits best with your needs and budget.

7)         Transfer Switches – These devices transfer your home’s electrical load from the utility line to the generator in the event of a power outage.  They should be matched correctly to the generator size, the amount of electrical load you expect the generator to back-up and they need to comply with local electrical building codes.  Your home’s electrical distribution panel is designed to carry a certain amount of electricity and the generator’s transfer switch should not allow more power than the distribution panel can handle.

8)         True, Clean Power – All generators create harmonic distortion which can interfere with sensitive electronic equipment such as high-end HVAC systems, plasma televisions and computers. The best generators produce less than five percent total harmonic distortion to ensure 100 percent compatibility with all household appliances.

9)         Ease of Installation – Installation of a standard residential standby generator should only take a matter of hours by a qualified installer. Some generator systems come with pre-wired transfer switches to make it simpler for the professional installer or a serious DIY’er.

10)      Dealer Network – A well-trained and well-qualified dealer is important not only when you first purchase and install the generator, but for years afterward for routine maintenance and service.  Make sure the dealer you choose is very familiar with standby generators and has an electrical background.  Generator manufacturers have widely varying dealer networks. The best ones give you many choices no matter where you live.

“It is very important to know all the facts before purchasing a standby generator,” says Clement Feng, executive vice president and chief marketing officer, Generac. “Generac offers a simple, user-friendly sizing tool on the Generac website which makes choosing the right generator for the home even easier.”

A Generac Guardian series unit offers the highest output of any generator of its kind at the most competitive price on the market – ranging from eight kW to 60 kW. What consumers may not know is that the Generac Guardian series of residential automatic standby generators is backed with 50 years of experience in the power generation industry. The power quality also is best in its class, allowing for safe operation of sensitive electronic equipment.

For more than 50 years, Generac has been in the business of making generators for both homes and businesses. “This is all we make and we pride ourselves in being the nation’s leader,” continued Feng. “And as a leader, we continue to set the bar for high-quality, high-performing backup power solutions.”

Generac introduced the first gaseous-fueled automatic home standby system in 1989 and has been the leading brand ever since. Generac is a proud supporter of the Home Safety Council and has earned the Good Housekeeping Seal after evaluation by the Good Housekeeping Research Institute. For more information on Generac residential and commercial products.

About Generac Power Systems, Inc.

Since 1959, Generac Power Systems, Inc., has been a leading, innovative manufacturer and marketer of portable and standby generators, automatic transfer switches, modular paralleling systems, and small engines for recreational vehicle, residential, and commercial applications. Generac’s power systems range in output from 1 to 9,000 kilowatts. Generac is a proud supporter of the Home Safety Council and earned the Good Housekeeping Seal in 2009.  For more information on Generac and its extensive line of both portable and automatic generators.

Accomplishments

In 2009 Generac® Power Systems was selected as the Waukesha County Business of the Year and was named a top Milwaukee workplace by the Milwaukee Business Journal. The Generac Liquid-Cooled Standby Generator was selected as one of Professional Builder’s 2009 “100 Best New Products.” The Generac Guardian Series 20 kW Air-Cooled Standby Generator was named one of Professional Builder’s  2008 “100 Best New Products;” was a finalist for the Building Products’ “2008 MVP Awards” and Electrical Contracting Products’ “2008 Innovation Award.” In addition to the GenReady Load Center Panel, the 20 kW Air-Cooled Standby Generator received Professional Remodeler’s 2008 “50 Most Innovative Products Award.” In 2007, Building Products named the Generac® 16 kW QuietSource commercial generator one of its “2007 Top Products.” Generac also received Building Operating Management’s “2007 Reader’s Choice Award” for the QT Series of commercial generators. The Generac Gemini® Twin Pack was a finalist for Consulting-Specifying Engineer’s “2008 Product of the Year” award. Since 2006, Generac has been a Better Business Bureau Accredited business with an A+ Business rating.