The most powerful electrical and mechanical design and sizing tool on the market, Generac Industrial Power’s Power Design Pro is a one stop solution center for the consulting engineer. In addition to state of the art generator sizing and analysis, it includes spec sheets, installation drawings, emission information, spec text library with full inclusive design notes, and the ability to link directly to your supporting dealer for budgetary quoting and additional support.
Generac Industrial Power has incorporated 50 years of power generation experience into Power Design Pro with the goal of making specifying generators as easy as possible. It incorporates state of the art algorithms that accurately model a load’s true characteristics and includes full harmonic and transient analysis to ensure complete generator to load compatibility. This ability to accurately size and design generator solutions is unmatched by any other software in the industry.
Compare Industrial Sizing Software | Competitor's Software | Generac Software | | Features | SpecSize | GenSize™ | Power Design Pro™ | | Sequence Control | | Multiple concurrent starting sequences | x | x | x | | Multiple non-concurrent starting sequences | | | x | | Multiple cyclic sequences | | | x | | Sizing Critia Based Upon | | Running & Peak kW | x | x | x | | Voltage dip (project limit) | x | x | x | | Frequency dip (project limit) | x | x | x | | Voltage dip (per sequence limit) | | | x | | Frequency dip (per sequence limit) | | | x | | Total harmonic voltage distortion (THVD) | | | x | | Load Modeling | | Basic (rkW, skW, rkVA, skVA) | x | x | x | | Advanced (harmonic spectrum analysis) | | | x | | Suggested voltage & frequency limits | | | x | | Suggested harmonic current spectrums | | | x | | Advanced modeling of SS, VFD, UPS, Chillers | | | x | | User defineable devices (customizable) | | | x | | Design Resources | | Specification text | x | x | x | | Specification text with design notes | | | x | | Drawing integration | | x | x | | Integrated request for quote & info functions | | | x | | Analysis Resources | | Generator sizing report | x | | x | | What if analysis | | | x | | Identify most demanding alternator loading | | | x | | Identify most demanding engine loading | | | x | | Harmonic Spectrum Analyzer | | | x |
| Installation Requirements |
True Harmonic Analysis
Current market sizing programs use simple rule of thumb multipliers to size the generator for non linear loads. Given the vast variation between different types of loads from different manufacturers, simple multiplier sizing is just not adequate for today’s complex loads. Power Design Pro utilizes harmonic analysis to limit the harmonic voltage distortion to acceptable levels. The program automatically selects an appropriate harmonic current signature for each load type but gives the user the ability to modify it to accurately model any load. Once the loads are entered, Power Design Pro calculates the resulting harmonic voltage distortion as that load is applied to various generators.

Accurate Load Modeling
Does your current sizing software ask questions applicable to your application, such as: Is the UPS technology passive, line interactive, ferro-resonant, or double conversion? Is the variable frequency drive input 6 pulse unfiltered, filtered, or IGBT? How many compressor motors are being utilized in that 100 ton chiller system and is reheat being applied?
Most sizing programs don’t. How can a load’s true nature be accurately captured without asking the pertinent questions? The Power Design Pro system approach expertly provides safe default settings when specific information is limited while incorporating applicable questions in order to model the load’s true characteristics. For unusual applications, Power Design Pro allows users to build their own load types inclusive of starting, running, and harmonic characteristics.
Load shedding
When designing redundant power solutions, load shedding schemes are often implemented to maintain system integrity. Power Design Pro provides the ability to shed loads that are entered into the program and allows the user to then evaluate the effects of running those loads against any generator configuration the user selects. The goal is not to simply provide a sizing recommendation, but provide an indepth analysis tool that allows the user to compare multiple scenarios for the best possibble solution.
Natural Load Sequencing, Cyclic Loading, and Load Factors
A common limitation and misapplication of traditional sizing programs occurs when too many loads are entered into a single step, resulting in a fictitious situation that assumes all the loads are running and starting simultaneously. To cope with this limitation, users were forced to manipulate the loads into some arbitrary load groupings. Power Design Pro easily overcomes this issue by supporting natural load sequencing, cyclic loading, and user definable load factors in addition to the traditional concurrent starting-load step method.
Installation Requirements
This application is installed on a per-user basis. The setup application will download and install the .NET Framework 2.0 if not already installed.
Required Software: .NET Framework 2.0., Internet Explorer 6.0 or later
Supported Operating Systems: Windows XP Service Pack 2, Windows 2000 Service Pack 3, Windows Server 2003, Windows Vista, Windows 7
Disk Space Requirements: 300 MB (x86), 630 MB(x64) disk space available
System Memory: 512 MB
Minimum Screen Resolution: 1024x768 (65k colors) (96 DPI)
Download Power Design ProTM
Installation Instructions
1. Download the application and run it
2. Follow the instructions on your screen until finished
3. Be sure to register your software to have access to all the benefits.
The application will check for updates each time it runs. If an update is available, it will be downloaded and installed automatically the next time you run the application. You must connect to the Internet and allow the application to check for updates at least once every 30 days in order to continue using the software.
By installing and/or running and/or using and/or distributing and/or modifying any part of this product you accept in full the responsibilities and obligations contained in the license whose text may be found in the file 'License.txt' in the distribution package.