Breadcrumbs

Home > 2014 > April > Generac Launches New MobileLink App
Generac Launches New MobileLink App

Generac Launches New MobileLink App

4/17/2014

Coverage of cellular remote monitoring system also expands to include Canada

Generac Power Systems, the market leader in automatic home standby power, unveiled a new mobile app for the popular Mobile Link™ cellular remote monitoring system at the International Builders’ Show on Feb. 4 in Las Vegas. The apps make it easier than ever for consumers to monitor their home standby generators using their mobile device.

“According to the Pew Research Internet Project, 86 percent of smartphone owners use their smartphone for ‘just-in-time’ information, like getting current traffic information or seeking help in an emergency,” said Jake Thomas, senior product manager for Generac. “Mobile Link and the new app are designed for these people. They want to know right away when their generator is running or when it needs maintenance. The Mobile Link app makes that information easier than ever for customers to get.”

The Mobile Link app is currently available for both iOS® and Android™ devices, and it’s free and downloadable on the iTunes™ App Store, Google Play™ and the Amazon Appstore.

Introduced in 2013, Mobile Link lets home standby generator owners view their generator’s status and maintenance needs, set the unit’s exercise schedule, review its running and maintenance history, and receive push notifications to indicate status changes. In June 2014, new functionality will be introduced that lets owners arrange to send notifications to their local dealer. This makes maintenance easier, since dealers can spot any issues in advance and can ensure the generator is operating smoothly, no matter the homeowner’s location.

Generator monitoring will continue to be available via the Web at www.standbystatus.com.

Mobile Link service has been expanded to include Canada. Previously available only in the United States, Mobile Link can now be used by the thousands of home standby generator customers throughout Canada, via the new app or the standbystatus.com website.

The Mobile Link device attaches in minutes to the outside of the Generac automatic backup generator enclosure and connects to the generator’s controller. Mobile Link sends data via cellular network because it is easier to configure and more reliable than the Ethernet and telephone connections used by many competitive monitoring solutions.

The Mobile Link device has an MSRP of only $279. The first year of cellular data is included with the purchase, after which homeowners can renew for $99 per year for a subscription, or at a discounted rate of $249 for a three-year subscription, less than many other competitive solutions.

Mobile Link is compatible with most Generac, Honeywell, Centurion, Siemens, and Eaton brand standby generators up to 20 kW manufactured from 2008, and 22 to 60 kW standby generators manufactured from 2010.

To learn more about Mobile Link, please visit www.standbystatus.com.