When writing your review, please consider the following guidelines:
- Prior to providing a review, refer to a product’s documentation to ensure that unit is being used and maintained properly
- Alluding to issues incurred in the wake of negligent maintenance or improper use will void review submissions
- Focus on your experience with the product and its features
- Provide details about why you liked or disliked a product
- Reviews submitted for products other than those listed will be rejected immediately
- Any product reviews referencing independent authorized dealers, service providers, or retailers by name will NOT be posted. (Dealer reviews can be provided here)
- All submitted reviews are subject to the terms set forth in our Terms of Use
We reserve the right not to post your review if it contains any of the following types of content or violates other guidelines:
- Obscenities, discriminatory language, or other language not suitable for a public forum
- Advertisements, “spam” content, or references to other products, offers, or websites
- Email addresses, URLs, phone numbers, product serial numbers, physical addresses or other forms of contact information
- Critical or spiteful comments on other reviews posted on the page or their authors
If you wish to share feedback with us about product selection, pricing, ordering, delivery, or other customer service issues, please do not submit this feedback through a product review. Instead, contact us directly.
Enjoy writing your review!
Rated 5 out of
5
by
BryanM from
Onewash still running great after 12 years
I purchased a Onewash when I bought my home 12 years ago to clean the driveway and it still is running great. The one issue I had recently is that the plastic female water hose connector on the pump appeared to be worn to a point where the hose kept falling off. I was ready to replace the pump but then thought since I got so many good years out of this pressure washer, why not just get a new one. As a last-ditch effort for a low cost solution, I purchased a brass 90deg 3/4" male to female hose connector and replaced the male connector on my hose and it worked! The engine still starts first pull after being stored for the winter and cleans great. Great quality and Made in the USA.
Date published: 2024-03-17
Rated 1 out of
5
by
dave from
Junk
Absolute Junk. Cant even locate parts to fix this piece of garbage. Used it 3 times to wash cars and clean a driveway and now it will not start or run.
Date published: 2024-02-03
Rated 5 out of
5
by
Jane45 from
This washer works great for all projects.
I have used the washer several times and have been impressed by how good it works. I have washed my house with good results. Also the driveway and the shed. The patio area cleaned up good too. So you can see I have used it for several big projects and it worked great each time. I am in my 70’s and had no problem using it.
Date published: 2023-11-16
Rated 1 out of
5
by
Ronrook from
Terrible.
Bought it three years ago- had to have warranty work done after the first use- worked great after warranty work- tried it today ( third time using it)- wouldn’t start. I had thought about getting a home generator in the future- no way would I go with a general.
Date published: 2023-10-10
Rated 5 out of
5
by
Gary57 from
Perfectly clean
Worked great , easy on gas and well put together , this is the second Generac purchase as I own a generator for the past 10 years so I knew it was a good company .
Date published: 2023-10-01
Rated 4 out of
5
by
krausweb from
Love the look and performance, but poor QC control from factory
Would give this 5 stars, but after the 3rd use, water started streaming out from the water pump. Found that three of the bolts that hold the water pump on had vibrated loose and allowed the water to damage the seal. Sent a support message to Gererac but have not heard back from them yet. Really like the unit and hoping to see Generac stand by their product by fixing the issue under warranty. I've only had the unit for 6 months.
Date published: 2023-09-24
Rated 2 out of
5
by
Homeowner from
Product not made ith easy to assemble parts. Hammers, pliers and wire brushes were needed and needed for assembly.
Product not made easy to assemble The parts required Hammers, pliers and wire brushes for assembly.
It appears that the quality of those parts are not what they should be.
I felt that buying an American product would be better.
Perhaps in the future GENERAC will get their products and parts from a more reliable manufacturer.
Date published: 2023-09-19
Rated 4 out of
5
by
David from
Short handle
I have had the pressure washer for 2 years, I really like this pressure washer, starts easy with the battery or the pull cord. The dial on the handle allows for several different pressures.
Need to make sure you have a 90 degree spout for your gas can or the gas will spill out.
I am 5’10” the handle needs to either be adjustable or longer, trying to guide the washer and maneuver it’s makes it difficult to pull, go down steps, or push.
Date published: 2023-09-10
OneWash Pressure Washer - 6602 is rated
4.5 out of
5 by
511.