Connecting the Generator to Your Home
Now that the generator is set, it’s time to connect to the fuel source. Your generator needs a fuel source, similar to your car or lawn mower. Generac generators can be fueled by liquid propane or natural gas. With either fuel source, a gas line will be laid underground that will connect from the liquid propane tank or natural gas meter to the generator. If the generator is a significant distance from the fuel source, additional trenching may be needed to ensure the gas line reaches the generator.
Take a Closer Look...
As your installer connects the gas line, you may notice these important connectors being used. Flex Fuel Lines, polypipe and flex risers, and shut-off valves are recommended to create a cost-effective and efficient connection. Shut-off valves are also required at the generator to provide an external fuel shut off for safety purposes. Some municipalities require a 24-hour leak test, which means starting the generator will have to wait until after the test is completed.
Next Steps
With the generator connected to a fuel source, it’s now time to connect it to your main electrical panel. Continue scrolling to the next section to learn about electrical connections.