Breadcrumbs

Home > Archive > Generac Power Systems Launches Smart and Affordable Backup Power Technologies
Generac Power Systems Launches Smart and Affordable Backup Power Technologies

Generac Power Systems Launches Smart and Affordable Backup Power Technologies

3/10/2015

Smart Management Module™ Increase Affordability; 16 Circuit NEMA 3R Transfer Switch reduces installation fees

Generac is pleased to announce that it has launched two new technologies that make installing an automatic home backup generator easier and more affordable for homeowners.

Generac’s new Smart Management Modules (SMM) are a load management system that allow homeowners to purchase a lower kilowatt automatic backup power system that fits within their budget, while the new 16 circuit NEMA 3R rated automatic transfer switch helps reduce installation costs for customers with an electrical panel located outside the home.

“As the preferred residential backup power provider, we understand that customers need affordable, quality solutions,” said Russ Minick, executive vice president of North American sales for Generac Power Systems. “The introduction of the Smart Management Modules and 16 circuit NEMA 3R transfer switch, are examples of our commitment to ensuring that automatic backup power systems are available for all homeowners.”

Smart Management Module (SMM)
Generac’s new Smart Management Modules (SMM) are a load management system that manages backup power to essential circuits identified by the homeowner, and autonomously pushes available power to non-essential circuits, as it becomes available.

The Smart Management Modules are wire-free, which makes them easier to install since no control wires are required, and helps lower installation costs. Up to eight Smart Management Modules can be installed with a compatible automatic transfer switch, to manage power loads. The Smart Management Module technology is protected in a NEMA 3R weather-proof enclosure, making each unit compatible for indoor and outdoor installations.  Additional features include an LED indicator light, which allows homeowners to verify which essential circuits are receiving power, as well as a lockout switch that prevents unwanted operation of circuits while operating on generator power.

New 16 Circuit Weather-Proof Automatic Transfer Switch
The new 16 circuit NEMA 3R rated automatic transfer switch is weather-proof, and can withstand high winds, rain, and winter storms. Electrical circuits are protected by an aluminum corrosion-resistant enclosure, and it accepts breakers from multiple manufacturers. Power can be provided to up to 16 essential circuits in a home by using this new transfer switch and customers can expand their backup coverage to 24 circuits, through the use of tandem breakers.

Prior to this introduction, homeowners without a basement or interior utility closet had to purchase a costly, custom-built subpanel that could be installed outside the home.

“Generac continues to invest significant resources into product development because of the important role of backup power products,” said Jake Thomas, Generac’s director of product management. “Today, power outages are less predictable, and are occurring more frequently for extended periods of time. Given this fact, the development of products that help customers control their power will continue to be the focus.”

Learn more about Generac's home backup generator transfer switch products.