Woman with generator outside and white picket fence.

When the power fails,  you won't.

A Generac home standby generator automatically restores power to your home during an outage, whether caused by storms, failed equipment or an overworked power grid, so your life goes on uninterrupted.

Our home standby generators provide permanent peace of mind. 

More ways to keep power close at hand.

At Generac, we believe everyone should have the power they need to tackle every chore, store the power they generate and bring the power they need on-the-go, wherever they go. So, we’ve built a wide range of products to do just that.  

An aerial view of a house on the left with lights on at night

Be the light when the rest of the block goes dark.

Not every power outage comes with a storm warning. There are plenty of things you can do now to prepare for when the power goes out, even when you don’t see it coming.

Proud to be powered by Generac.

Your trust is earned. 

We’ve worked hard to be your trusted source of power since 1959.

  • ENERGY STAR®

    2022 Partner of the Year

  • Grid Forward

    Annual Grid Innovator Award

  • Newsweek

    America’s Most Trustworthy Companies