Breadcrumbs

Home > Service & Support

Connecting Your Home Standby

How to Connect Your Home Standby

 

  • On your controller, press OFF then Escape to access the Main Menu 
  • On your controller, Select "Setup WiFi" and press Enter
  • The generator will display "Starting WiFi" for a few moments
  • The generator will display "Setup WiFi" again to confirm, select "Yes" then press Enter

 

1.  On Your Generator
2.  On Your Mobile Device


Connect to the MLG Network

A message may appear saying "Internet may not be available" - this message is expected, and is nothing to worry about.

 

 

  • Type 192.168.51.1 in the address bar on your mobile device and click enter
  • Select your country and time zone then click "Next"
  • Select your Wi-Fi network and enter your password (click "Show" to verify that the password entered is correct), then click "Connect"
  • If you are using a booster, be sure to connect to your booster rather than your Wi-Fi

 

3.  On Your Mobile Device
4.  On Your Mobile Device & Your Generator
  • When your generator displays "Now connected to:" press Enter
  • When your phone shows "You're connected!" this means your generator is connected and communicating.
  • Your generator should automatically obtain the time zone. Press Enter to continue. 
  • The screen on your generator will suggest an update via USB or Wi-Fi - press Escape to skip (the update will occur on it's own in the background.) 

**If the Wi-Fi signal is less than 40% and there are communication issues, a booster may be recommended.  See our recommended booster below or contact an Authorized Generac Dealer to purchase a compatible booster.  If you are using a booster, be sure to connect to the booster rather than your home Wi-Fi.**

Recommended Booster


Check your e-mail for your Free Mobile Link account information and log in to your Mobile Link Account!


Learn more about Mobile Link and upgrading to our Mobile Link Active Subscription and the features it offers!

  Log In to Mobile Link
Now What