This promotional offer is only valid January 23, 2023 – February 26, 2023. Offer valid only on qualifying home standby generator purchases made in the Houston, Texas Designated Market Area (DMA), as defined by Nielsen Holdings PLC. For a full list of zip codes within the DMA eligible to participate in this promotion, visit
www.Generac.com/Houston?cid=halo. Offer redeemable only when customer requests a free quote through the Generac Power Systems’ Consumer Sales Team, and purchases and installs a qualifying unit with an authorized, participating dealer** during the promotional timeframe. All eligible customers must have their generator installed and activated by May 7, 2023 to qualify for the promotion. Previous purchases are not eligible. Offer is not available through retail, wholesale, .com or other outlets, including dealers that do not participate in Generac’s Power Play program. Refurbished products are excluded from this offer. Generator must be installed and activated for the warranty to be applied. Individual prices may vary. The free promotional items are a 7-year extended warranty, one year of dealer maintenance, and one year of dealer monitoring – a $1,335 value. Dealer monitoring only covers remote monitoring of the unit. Generac Power Systems provides the 7-year warranty, and the 1st year of maintenance is provided by the Generac dealer that sold and installed the unit; must be one and the same. The maintenance offer is limited to a one-time visit by the installing Generac dealer to conduct maintenance and includes: Inspection of fuel connections and battery terminals, and replacement of oil, oil filter, air filter and spark plugs. Generac disclaims all responsibility for provision of the 1st year of maintenance. The generator must be connected to an active internet source (Wi-Fi, Ethernet, or Cellular). Connectivity results may vary based on communication device and geographic location. If generator becomes disconnected from an internet source, customer is responsible for reconnecting the generator. Generac is not responsible for costs associated with reconnecting generator to internet source, by a third party. Limit one promotional offer per installed generator. Only Generac Guardian Air-Cooled Home Standby Generators 10kW – 26kW are eligible for this offer.
**A participating authorized Generac dealer is a member of Generac Power System’s PowerPlay Program. All quotes must be scheduled through Generac’s Consumer Sales Team, and all purchases must be made through a PowerPlay dealer to qualify for the promotion.
Click here to view eligible zip codes.