Breadcrumbs

Home > Resources and Tools > CE Installer Resources > Installation Resources

Installation Resources

PWRcell Installation Resources

Resources for installers in the field

Important: Installation Checklists


1.  Pre-Installation Checklist

Review and complete the pre-installation checklist to avoid common user errors on site.
 


2.  Post-Installation Checklist

Complete this checklist to ensure warranty registration and compliance with local utility.
 
 

PWRCELL STORAGE FOR PROTECTED LOADS BACKUP

See how the battery rating will impact the design of the backed up loads.

This example sheet will walk you through how to use the worksheets.
PWRcell Example Worksheet Breakout
 

Select the applicable loads worksheet for your design.
 
Protected Loads Breakout M3

Protected Loads Breakout M4

Protected Loads Breakout M5

Protected Loads Breakout M6


Generac's Residential Loads Table


NOTE: It is important to consider the continuous power rating of the battery.  In the event of an outage, the battery is the only source to support the system and loads.

 

Return to the Top of the Page

TIME OF USE PROGRAM GUIDE

Setup guide for Time of Use (TOU) for your region and utility
How to configure your inverter for TOU from a given set of TOU codes

PWRcell TOU Guide

Return to the Top of the Page

PWRcell Registration

Register PWRcell to Activate the 10 Year Warranty!

1.  Install the inverter
2.  Connect it to the internet
3.  Go to: PWRfleet.generac.com
4.  Create a FREE account
5.  Start using PWRfleet to register and monitor all of your customer's sites


 

Return to the Top of the Page

Firmware Updates

Get the latest firmware to unlock new features and improved performance, and to ensure proper operation with the new PWRcell ATS, SMMs, and 3.0kWh PWRcell Battery Modules.

TO UPDATE PRODUCT FIRMWARE, FOLLOW THESE EASY STEPS:

1.  Install, commission and register PWRcell system - reference the Quick Start Guide.

2.  Verify that the system is connected to the internet.

3.  If commissioning the system during business hours (8AM-8PM ET, M-F) Call 1-855-395-7841 for immediate firmware update.

4.  If commissioning outside of business hours, fill this form to receive an automatic firmware update.

Your request will be serviced in the order that it is received and the update will be completed within 24hrs.

Return to the Top of the Page

More Job-Site Resources