Nature is beautiful. So is a hot cup of coffee in the morning.
Camping is all about experiencing the outdoors, but that doesn’t mean you have to leave behind the small comforts. A portable power source isn’t just backup for emergencies. It’s a dependable companion that lets you bring the best of home to all the wild places that inspire you. Whether you're backpacking under the stars or setting up a full-fledged RV basecamp, reliable power means you can keep your camera charged for that perfect sunset shot, light up the campsite after dark, and stay connected with the outside world—whatever it takes to make your adventure great.
If you’re considering a portable power source, you can start by determining which category is right for you: gas or electric.
Inverter generators: Dependable, high-output, and great for extended stays—but they require fuel and can be noisy. They’re well-equipped to handle the larger loads that come with family-sized RVs or multiple sites.
Portable power stations: Silent, lightweight and emission-free—but they have limited runtime without solar attachments or a recharge. They’re ideal for tent or car camping.
Portable power exists for all those times when nature won’t cooperate. No matter what kind of portable you have, it will provide comfort in any condition. If temperatures dip below freezing, you can regulate the temperature in your camper, outfit your tent with a small heater, or snuggle up with an electric blanket. Or, if a heatwave threatens to spoil your weekend getaway, an AC unit will keep you cool at night and offer a much-needed reprieve during the day. Traditionally, campers have relied on fire. But if wood is waterlogged or scarce, you can count on a portable power source to provide power for heat and the means to prepare food instead.
Portable generators have become a common sight at campgrounds for all these reasons and more. But there’s one thing holding some campers back: no one wants to be “that guy” at the campground, the one disturbing the peace with a loud, clunky engine. Fortunately, today’s portable generators are quieter and more efficient than ever. Generac models like the iQ3500 or the GP2500I are specifically designed for dramatically lower noise levels. Better yet, portable power stations are almost completely silent. are almost completely silent. You can sleep right next to one without noticing the hum. And that’s the other plus—they’re 100% electric and emission free, safe to use in your tent or RV. You’ll have no problem running them in enclosed spaces or around others. Ultimately, portable power means freedom. Concerns about discomfort or staying connected can keep you tethered to crowded campsites. But if you always have an outlet on hand, you can venture out beyond the beaten path without worrying about your next charging opportunity.
Roughing it in the great outdoors is an exciting challenge when you’re on your own. Going off-grid with your family in tow, on the other hand, is a completely different story—especially when kids are involved. It can be tough to strike the right balance. The goal is to help them truly experience and appreciate nature. But sometimes, conditions get uncomfortable and classic activities lose their shine. Pushing them too hard could end with a mad dash for the car—if your family isn’t having fun, what’s the point of staying?
Don’t accept defeat by ending your trip early. Instead, prepare for less-than-ideal conditions by bringing a backup plan that can offer security, comfort and entertainment when needed. With a power source, you can keep your electronic devices charged and ready to go for emergencies—or emergency movie nights, if the mood strikes. And if the weather gets frigid or hot and sticky, you’ll have options.
There are mealtimes to think of as well. Cooking over an open fire will never go out of style, but you might find yourself craving some variety after a day or two of hot dogs. Imagine starting your morning with the smell of bacon and coffee—passing around plates piled high with sizzling hot food, served straight off the electric griddle. Camp stoves, electric kettles and other portable appliances can take your campsite meals to a whole new level. You don’t need to lug a cooler full of ice around to keep your food fresh, either. With a reliable power source on hand, you can pack a small fridge with milk, eggs and all the perishables you’d typically do without. Good food is fuel for the greatest adventures—so give your family a feast worth remembering.
"Bought this generator to power my RV for off grid camping. ... Starts like a dream and easily powers my AC and other things. Runs very quiet on economy mode."
- Generac Owner, Calgary, AB
Your portable power source isn’t just good for protecting your fun, either. With a little imagination, it can become a key feature of the good times. You can use it to:
The possibilities are endless.
At the end of the day, camping is about freedom—the freedom to explore, unwind and create unforgettable memories. A portable power source doesn’t take away from the adventure; it enhances it, giving you the flexibility to camp how you want, where you want.
Whether it’s keeping the essentials running, adding a little comfort, or bringing some extra magic to your nights under the stars, reliable power means nothing can hold you back. So, go ahead. Find the option that’s right for you, and use it to venture farther, stay longer and make every moment count.