Breadcrumbs

Home > Global Monitor > Current Articles > News from Italy & Europe
News from Italy & Europe

News from Italy & Europe

10/5/2017

Dealer News
 
GENERAC MOBILE PRODUCTS INKS DEAL WITH LEADING NORDIC CONTRACTOR
 
To further strengthen its existing product portfolio and improve its mobile power solutions, Generac Tower Light® has signed an exclusive dealer agreement with El-Björn AB, the leading construction and electrical contractor in Swedish and Norwegian territories.
 
Having operated in these territories for over a decade, Generac Tower Light looks forward to its union with El-Björn AB and the unrivaled comprehensive product and servicing package it will create for customers, such as construction companies and electrical contractors. To relieve the pressure of finding temporary solutions that are both efficient and sustainable, El-Björn AB will introduce a variety of new products as part of its agreement with Generac Tower Light. This will include the efficient V20 light tower, the ultra-compact Linktower T3 and the Linktower T3 UFO, a revolutionary 360° soft light most recently introduced to European markets. Easy to maintain and service, all products will be made available to construction and direct hire markets throughout 2017 and beyond, and will be supported by maintenance and service capabilities.
 
El-Björn AB is based in Sweden and currently employs 115 people. The company manufactures and provides comprehensive solutions for power, lighting and climate control to a broad group of mobile power consumers.
 
Generac Tower Light is enthusiastic about the opportunity this new relationship presents and looks forward to future success for both companies in the years to come. To learn more about El-Björn AB, click here.
 
 
 
  
New Product Introductions
 
NEW LIGHTING SOLUTIONS FROM GENERAC TOWER LIGHT FEATURE ENHANCED LIGHTING POWER
 
In an effort to provide enhanced illumination capabilities to a variety of unique applications, Generac Tower Light has introduced a 360° mobile lighting solution to the light tower market. The company’s new UFO product line combines the power of two light tower models: the engine-powered MT1 RT UFO Linktower and the Linktower T3 UFO, which can be powered by an external power source like a power generator or alternative light towers featuring built-in generators. Both of these light tower models are equipped with 400W rounded LED floodlights and illuminate wide areas with 50,0000 lumens of lighting power without bothersome glare. Ideal for road work, contruction sites or outdoor events, these models can be linked together to form a superior lighting solution that operates on a single power source.
 
For more product specs on either of these two new product models, click here.

 
  
Upcoming Events
 
GMP TO SHOWCASE DUST CONTROL AND WASH RACK SOLUTIONS AT MAJOR EVENT THIS NOVEMBER
 
From 7-10 November, Generac Mobile Products® will travel to Rimini, Italy, to exhibit at Ecomondo 2017. As a tradeshow designed for Italian and foreign companies to view and present the mobile power market’s latest innovations and technologies, Ecomondo 2017 provides an ideal venue for Generac Mobile Products to display a variety of the company’s innovative product models to consumers, industry enthusiasts and mobile power professionals.
 
Generac Mobile Products plans to showcase a variety of dust control units, including its DF15000 and DF Smart product models. The company also looks forward to unveiling a brand new dust control unit at this year’s show. Several representatives from Generac Mobile Products will be on hand to discuss the dust control capabilities of their existing product line, which includes indoor jobs like asbestos removal and outdoor applications such as demolition sites and rock quarries.
 
In addition to these dust control solutions, representatives will also be displaying models from the company’s wash rack product line. Wash rack models feature special washing bays for construction machinery, heavy duty equipment and a variety of industry tools, which can be cleaned through a cost-efficient filtering system that features a closed-loop water source to cut-down on cost and unnecessary waste.
 
To view these environmentally friendly products first-hand and discuss industry trends with Generac Mobile Products’ representatives, visit us at Stand 122 in Hall C5 of the Rimini Expo Center. Find additional information on this annual event here.
 
 
 




News from Mexico, Brazil, and Rest of Latin America