Introduction
In an era of increasing environmental consciousness and tightening regulatory frameworks, the choice of power generation technology carries significant implications. This white paper explores the distinct environmental and regulatory advantages offered by natural gas generators, positioning them as a superior solution for both emergency standby and non-emergency power needs. By examining their cleaner-burning properties, lower emissions profile (compared to diesel generators), and streamlined compliance process, we demonstrate why natural gas generators are often a preferred choice to help businesses maintain sustainable and compliant operations.
Cleaner-Burning Properties and Reduced Emissions
Natural gas stands apart from traditional fossil fuels, particularly diesel, due to its inherently cleaner combustion characteristics. Composed primarily of methane, natural gas burns more completely and efficiently, resulting in a significantly reduced output of harmful pollutants.
Key emission advantages of natural gas generators as compared to diesel include:
These inherent properties make natural gas a fundamentally cleaner fuel source, providing a clear environmental benefit over other common generator fuels. On average, Generac’s natural gas generators emit 95% less NOx emissions, 98% less NMHC emissions, and 59% less CO emissions as compared to equivalent diesel generators. Over the lifetime of the equipment, this results in significantly less emissions. See graph below:

See Appendix for calculation logic and assumptions
Alignment with Increasingly Stringent Environmental Regulations
The global trend towards stricter environmental regulations, driven by concerns over climate change and public health, places a premium on low-emission technologies. Natural gas generators are uniquely positioned to meet and exceed these evolving standards.
The inherent cleanliness of natural gas as compared to diesel helps ease the path to regulatory compliance, future-proofing investments in power generation infrastructure against tightening environmental mandates.
Navigating Fuel Source Requirements: NFPA 70 and NFPA 110
The National Fire Protection Association (NFPA) codes, specifically NFPA 70 (National Electric Code) and NFPA 110 (Standard for Emergency and Standby Power Systems), provide guidance for emergency power systems. However, guidance
regarding fuel sources requirements can sometimes appear ambiguous or even contradictory, leading to confusion among specifiers and Authorities Having Jurisdiction (AHJs).
Despite the perceived ambiguities in these standards, many AHJs across the United States have accepted and approved natural gas-fueled engines for emergency power systems. Historically, only on-site diesel storage would have been allowed. This increase in AHJ acceptance is driven by a practical understanding of natural gas infrastructure reliability, coupled with the environmental benefits. The aftermath of natural disasters like Irene and Sandby helped prove the resilience and improved the acceptance of NG as an acceptable source for emergency and life-safety systems. NFPA NEC 70 Chapter 7 Section 700.12(C)(3) allows natural gas as an acceptable fuel “where there is a low probability of simultaneous failure of both the off-site fuel delivery system and power from the outside electrical utility company.”
Examples of AHJ Acceptance
This growing trend reflects a pragmatic approach by AHJs, recognizing that the reliability and environmental advantages of natural gas can meet the intent of emergency power requirements, even when the prescriptive language might seem
to lean towards on-site fuel storage.
Regulatory Landscape, Permitting Considerations, and Ease of Compliance
Navigating the regulatory landscape for power generation equipment can be complex and time-consuming. Natural gas generators offer a comparatively smoother path to permitting and compliance for both emergency standby and non-emergency applications.
The established infrastructure for natural gas delivery also simplifies fuel supply logistics, further contributing to operational ease and compliance.
Conclusion
Natural gas generators present compelling environmental and regulatory advantages that make them an increasingly attractive choice for modern power generation. Their cleaner-burning properties lead to significantly lower emissions of NOx, CO, and virtually no particulate matter, aligning seamlessly with the growing demand for cleaner air and sustainable practices. This superior environmental performance (as compared to diesel) translates directly into a more favorable regulatory landscape, simplifying permitting processes, helping reduce compliance burdens, and offering greater operational flexibility for both emergency standby and non-emergency applications. By choosing natural gas, organizations can achieve reliable power while demonstrating a commitment to environmental stewardship and helping ensure long-term regulatory compliance.