Breadcrumbs

Home >

Generac Recalls Portable Generators Due to Finger Amputation and Crushing Hazards

Release Date: July 29, 2021
Recall Number: 21-173

Recall Summary

Name of Product: Generac® and DR® 6500 Watt and 8000 Watt portable generators

Hazard: An unlocked handle can pinch consumers’ fingers against the generator frame when the generator is moved, posing finger amputation and crushing hazards.

Remedy: Repair

Consumers should immediately stop using the recalled portable generators, unless the locking pin has been inserted to secure the handle in place before and after moving the generator, and contact Generac for a free repair kit.

Consumer Contact:

Generac toll-free at 844-242-3493 from 8 a.m. to 5 p.m. CT Monday through Friday, or online at www.generac.com/handleguard or www.generac.com and click on Important Safety Information for more information.

 

Recall Details

Units: About 321,160 (In addition, 4,575 in Canada)

Description: This recall involves 6500 watt and 8000 watt Generac portable generators with unit type numbers XT8000E XT8000EFI, GP6500, GP6500E, GP8000E and HomeLink 6500E portable generators, and DR models PRO 6500M and PRO 6500E portable generators. The generators have gasoline-powered engines that are used to generate electricity for use as backup power. The portable generators have two-wheels and a single, U-shaped, two-grip, flip-up pin-lock handle to help move the generator. Only the generators listed below are included in this recall. The unit type is identified on the front of the product. The model and serial numbers are printed on a label on the product. Consumers can also check specific unit type, model number, and serial number location information at www.generac.com/service-support/product-support-lookup.

Incidents/Injuries: Generac has received eight reports of injuries, seven resulting in finger amputation and one in finger crushing.

Sold at: Major home improvement and hardware stores nationwide and online, including Ace Hardware, Amazon, Blain’s Farm & Fleet, City Electric Supply, Costco, Do it Best, Fastenal, Home Depot, Lowe’s Stores, Napa Auto Parts, Northern Tool & Equipment, Orgill, Power Equipment Direct, Ravitsky Bros., True Value, and W.W. Grainger from June 2013 through June 2021 for between $790 and $1,480.

Manufacturer: Generac Power Systems, of Waukesha, Wis.

Manufactured in: United States and China

Note: Health Canada's press release is available at: https://healthycanadians.gc.ca/recall-alert-rappel-avis/hc-sc/2021/76007r-eng.php

Photos


Recalled XT8000E Generator

Recalled XT8000EFI Generator

Recalled GP6500 Generator

Recalled GP6500E Generator

Recalled GP8000E Generator

Recalled PRO 6500M Generator

Recalled PRO 6500E Generator

Recalled Homelink 6500E Generator

About the U.S. CPSC
The U.S. Consumer Product Safety Commission (CPSC) is charged with protecting the public from unreasonable risks of injury or death associated with the use of thousands of types of consumer products. Deaths, injuries, and property damage from consumer product incidents cost the nation more than $1 trillion annually. CPSC’s work to ensure the safety of consumer products has contributed to a decline in the rate of deaths and injuries associated with consumer products over the past 40 years.

Federal law bars any person from selling products subject to a publicly announced voluntary recall by a manufacturer or a mandatory recall ordered by the Commission.

For lifesaving information: