Pressure Washer Safety Campaign

Redeem
U.S. Consumer Product Safety Commission – Fast Track Recall with Health Canada

Release Date: May 14, 2026

Generac Power Systems Expands Recall of Generac and DR Power Electric Start Pressure Washers Due to Risk of Serious Injury or Death from Carbon Monoxide Hazard; Includes Additional Models  

Recall Summary

Name of Product: Electric Start Pressure Washers

Hazard: The electronic start/stop button on the pressure washer can malfunction and self-start, posing a risk of serious injury or death due to carbon monoxide poisoning if the unit is in a confined space.

Remedy: Repair

Consumers should immediately stop using the recalled pressure washer unless they have removed the rechargeable battery and contact Generac to arrange for a free of charge repair at your dealer’s location. The pressure washer can continue to be used with the battery removed by using the pull-start option to start the unit.

Consumer Contact: Generac Power Systems toll-free at 800-396-9047 from 8 a.m. to 5 p.m. CT Monday through Friday, or online at www.generac.com and click on “Important Recall Information”  at the bottom of the page or go to https://www.generac.com/about/recalls/pressure-washer for more information.

Recall Details

Units: About 16,260 (Generac Power Systems previously recalled 53,000 units on April 28, 2022.) (In addition, about 120 were sold in Canada)

Description: This recall involves Generac brand electric start pressure washers with model numbers G0088941 (serial numbers 3010751056 through 3012693273 only), G0088951 and G0089111 and DR Power brand electric start pressure washers with model number DPW3109DEN. The pressure washers have an electric start/stop button for the unit’s gasoline-powered engines, as well as a rechargeable battery used to power the button. Model and serial numbers are printed on a label located on the product’s frame. Consumers can check specific unit type, model number and serial number location information at https://www.generac.com/support/product-info-user-manuals by clicking on “Pressure Washers”  at the bottom of the page.

Incidents/Injuries: The firm has received six reports of the pressure washers self-starting.  No injuries or property damage have been reported.

Sold at: Major home improvement and hardware stores online and nationwide including Menards, Home Depot, and Amazon from November 2021 through February 2026 for between $500 and $590.

Manufacturer: Generac Power Systems Inc., of Waukesha, Wisconsin

Manufactured in: United States

Notes: Health Canada's Press release is available at: https://recalls-rappels.canada.ca/en/alert-recall/generac-power-electric-start-pressure-washers-recalled-due-carbon-monoxide-poisoning  

 

Material Description Last Serial #
DPW3109DEN DR Pressure Washer PRO 3100 All
G0088941 3125 CON GAS PW ES CARB EPA3 3010751056 3012693273
G0088951 3125 CON GAS PW ES SPEEDWASH CARB EPA3 All
G0089111 3125 GAS PW ES EPA3/CARB G32 All

 

Photos

Recalled Generac Model G0089111

Recalled Generac Model G0088941

Recalled Generac Model G00088951

Recalled DR Power Model DPW3109DEN

 

Fast Track Recall

About the U.S. CPSC
The U.S. Consumer Product Safety Commission (CPSC) is charged with protecting the public from unreasonable risk of injury associated with the use of thousands of types of consumer products. Deaths, injuries, and property damage from consumer product-related incidents cost the nation more than $1 trillion annually. Since the CPSC was established more than 50 years ago, it has worked to ensure the safety of consumer products, which has contributed to a decline in injuries associated with these products.

Federal law prohibits any person from selling products subject to a Commission ordered recall or a voluntary recall undertaken in consultation with the CPSC.

For lifesaving information:

- Visit CPSC.gov.

- Sign up to receive our e-mail alerts.

- Follow us on Facebook, Instagram, X, BlueSky, Threads, LinkedIn and Truth Social.

- Report a dangerous product or a product-related injury on www.SaferProducts.gov.

- Call CPSC’s Hotline at 800-638-2772 (TTY 301-595-7054).

- Contact a media specialist.