There are no current Promotions/Recalls

U.S. Consumer Product Safety Commission – Fast Track Recall with Health Canada

Generac Power Systems Recalls Portable Generators Due to Serious Risk of Injury or Death from Burn and Fire Hazards

Recall Summary

Name of Product: Generac Portable Generators

Hazard: When first filling the recalled generator with gasoline, fuel can leak from the carburetor posing a serious risk of injury or death from fire or burn hazard. Consumers with generators that have previously been filled with enough gasoline to move the gauge off "E," or have been used without any gasoline leakage, can continue use.

Remedy: Repair

Consumers should immediately stop using the recalled Generac portable generator and go to at https://www.generac.com/about/recalls/GP-Carburetor to check to see if your model and serial number are included in this recall. If your unit is included in the recall and has either not yet been filled with fuel or exhibited leakage after fueling as described above, please contact your dealer to arrange for free repair at the dealer’s location.

Consumer Contact: Generac toll-free at 800-396-9951 from 8 a.m. to 5 p.m. CT Monday through Friday or online at https://www.generac.com/about/recalls/GP-Carburetor or www.generac.com and click on “Important Recall Information” for more information.

 

Recall Details

Units: About 149,400 (In addition, about 260 were sold in Canada).

Description: This recall involves certain Generac Portable Generators which have an orange/black cover and are incased in a steel-tube cradle. It comes with two wheels on the back for easy transportation. 

“Generac” and the “unit type” are located on the side panel of the generators. The model and serial number are printed on a label attached to the side of the unit. Consumers will need to have their model and serial number available prior to logging on to https://www.generac.com/about/recalls/GP-Carburetor to determine if their generator is included in the recall.

Recalled unit types and model numbers are listed below, within limited serial range.

 

Unit Type 

Model Number 

Serial Range 

GP3600 

G0077210 

3016697885–3016702012 

GP4000 DF 

G0081550 

3016000801–3016005506 

 

 

3016211528–3016216905 

 

 

3016218754–3016226593 

 

 

3016449617–3016450762 

 

 

3016451270–3016453540 

 

 

3017247749–3017247756 

 

 

3017281304–3017282335 

GP6500 

G0076802 

3016071245–3016073356 

 

 

3017019945–3017022257 

 

 

3017271028–3017271795 

GP6500 

G0076722 

3016064523–3016065290 

 

 

3016067789–3016069708 

 

 

3017268724–3017269491 

GP6500E 

G0077130 

3016524272–3016525039 

GP6500E DF 

G0081530 

3015996961–3016000800 

 

 

3016170144–3016185749 

 

 

3016186869–3016188514 

 

 

3016188590–3016190125 

 

 

3016190147–3016195522 

 

 

3016195727–3016196494 

 

 

3016196895–3016199198 

 

 

3016200968–3016207111 

 

 

3016207880–3016211527 

 

 

3016798879–3016800414 

 

 

3017276695–3017280535 

GP6700E DF 

G0080620 

3016125328–3016135133 

 

 

3016135902–3016141091 

 

 

3016141862–3016146661 

 

 

3016366592–3016369670 

 

 

3016788967–3016791273 

 

 

3017027309–3017034222 

 

 

3017034540–3017035307 

 

 

3017275351–3017276694 

GP8000E 

G0077150 

3016051079–3016054343 

 

 

3016056456–3016058184 

 

 

3016779444–3016784053 

 

 

3017025767–3017027302 

 

 

3017273815–3017275350 

GP8000E 

G0076754 

3016702013–3016702780 

 

 

3016777323–3016779434 

 

 

3017269492–3017271027 

GP8000E 

G0081540 

3016710640–3016715247 

 

 

3016800991–3016806368 

GP9200E 

G0079712 

3016786070–3016788388 

GP9500E TF 

G0080630 

3016708891–3016710618 

                                               

 

3016791274–3016793583 

Incidents/Injuries: The firm has received 114 reports of generator fuel leaks. No injuries have been reported.

Sold at: Home Depot, Lowe’s and other home improvement and hardware stores nationwide and online from May 2025 through February 2026 for between $600 and $1,300. Importer: Generac Power Systems Inc., of Waukesha, Wisconsin

Manufactured in: Vietnam

Notes: Health Canada's press release is available here in English and here in French.

If you find that your generator is not part of the recall and you are having maintenance and/or other questions with it, go to https://support.generac.com/s/topic/0TO5f000001KWfNGAW/portable-power for FAQs

Based on available information, no more than 51,500 units were distributed to consumers.

Recalled Generac Portable Generator GP8000E, model G0077150

  Recalled Generac Portable Generator GP6700E DF, model G0080620  

Recalled Generac Portable Generator GP6500E DF, model G0081530

  Recalled Generac Portable Generator GP6500, model G0076802  

 

Recalled Model and Serial Number Location– models G0077210, G0081550, G0081530, G0080620, G0080630

 

Recalled Model and Serial Number Location – models G0076802, G0076722, G0077130, G0077150, G0076754, G0081540, G0079712

 

Detailed View of Product Label with Model and Serial Number

 

Fast Track Recall

About the U.S. CPSC
The U.S. Consumer Product Safety Commission (CPSC) is charged with protecting the public from unreasonable risk of injury associated with the use of thousands of types of consumer products. Deaths, injuries, and property damage from consumer product-related incidents cost the nation more than $1 trillion annually. Since the CPSC was established more than 50 years ago, it has worked to ensure the safety of consumer products, which has contributed to a decline in injuries associated with these products.

Federal law prohibits any person from selling products subject to a Commission ordered recall or a voluntary recall undertaken in consultation with the CPSC.

 

For lifesaving information:

- Visit CPSC.gov.

- Sign up to receive our e-mail alerts.

- Follow us on Facebook, Instagram, X, BlueSky, Threads, LinkedIn and Truth Social.

- Report a dangerous product or a product-related injury on www.SaferProducts.gov.

- Call CPSC’s Hotline at 800-638-2772 (TTY 301-595-7054).

- Contact a media specialist.