When writing your review, please consider the following guidelines:
- Prior to providing a review, refer to a product’s documentation to ensure that unit is being used and maintained properly
- Alluding to issues incurred in the wake of negligent maintenance or improper use will void review submissions
- Focus on your experience with the product and its features
- Provide details about why you liked or disliked a product
- Reviews submitted for products other than those listed will be rejected immediately
- Any product reviews referencing independent authorized dealers, service providers, or retailers by name will NOT be posted. (Dealer reviews can be provided here)
- All submitted reviews are subject to the terms set forth in our Terms of Use
We reserve the right not to post your review if it contains any of the following types of content or violates other guidelines:
- Obscenities, discriminatory language, or other language not suitable for a public forum
- Advertisements, “spam” content, or references to other products, offers, or websites
- Email addresses, URLs, phone numbers, product serial numbers, physical addresses or other forms of contact information
- Critical or spiteful comments on other reviews posted on the page or their authors
If you wish to share feedback with us about product selection, pricing, ordering, delivery, or other customer service issues, please do not submit this feedback through a product review. Instead, contact us directly.
Enjoy writing your review!
Rated 5 out of
5
by
FlyESLA from
The Generac 3100psi pressure washer is the best.
I have used mine for a year now. The electric start makes this easy for anyone to use. My wife even likes using it when undertaking one of her cleaning projects.
Date published: 2022-07-23
Rated 5 out of
5
by
Truck102 from
This unit seems to be well built with good material compared to other washers in its class
Assembly was very easy and quick. First time to use it out of the box it was 95 degrees and and did my deck and whole house off and on for about 6 hours. It performed well. The electric power cord is plenty long. For an electric pressure washer it handles small jobs well.
Date published: 2022-07-18
Rated 5 out of
5
by
BILLD69 from
[Nice machine for the price
Good quality machine for a fair pricemy 15. THIS is my 3rd machine I had 2 machines previously for my 15 year HANDYMAN Business THE held up like gold. No complaints here. Now retired I bought another one electric start for around the house to use for different reasons and in my hobby of auto and truck restoration. IF THEY WERE JUNK BELIEVE ME I WOULD NOT BE AFRAID TO SAY THAT ALSO. BUT WHEN SOMETHING IS QUALITY AND A GOOD DEAL FOR MY HARD EARNED MONEY I WILL PROMOTE IT ALL DAY LOSO THATS MY STORY AND IM STICKING TO IT. NG.
Date published: 2022-07-03
Rated 4 out of
5
by
FricknMo from
Powerful yet flawed product
Negatives:
#1. Let me start with engineering. They don't make access to the engine oil very easy. Hard to fill the oil without a funnel.
#2. The Uberflex Hose isn't very flexible. Flexzilla hose is more flexible, but it is better than other power washers.
#3 The owner's manual is terrible. Instructions are not very clear.
#4 If you use the pull starter there should be an area to put your foot to hold down the unit.
#5 Should have included a Turbo Nozzle for the price.
Positives
#1 Powerful.
#2 Made in the USA
#3 Battery starter.
Date published: 2022-05-30
Rated 5 out of
5
by
Dirty68 from
Electric start!!!!
Got this for my wife. Electric start is the only way to go. Great features! She loves it and so do i.
Date published: 2022-05-26
Rated 3 out of
5
by
CapitalMess2022 from
Bought Generac expecting higher quality - was wrong
So I've owned this PW for approx 3 years. The first year I used it, I was quite impressed with the features/quality of the build. However I did notice the start/stop button was finicky.
Year 2, the electric start was mediocre at best with probably working every 1 out of 3 attempts. I ultimately would result on pull starting it.
Now in year 3, its exclusively a pull start and even that doesn't work well. I've spent sometimes in excessive of 15mins getting this to turn over.
Now let me be honest, once this thing is running, it works extremely well. Solid motor and pump system, good features etc and I've used it for everything from cleaning my boat, my driveway, siding, and washing my deck.
But, to be honest getting this pig to run and investing 15 mins to get it running to do a 10 min job makes me want to push it to the curb. But I'm mechanically inclined and too stubborn to let the machine win so I do this ritual every time and finally get it running.
Now I've learned there is a recall on the start/stop switch for safety reasons. The instruction is to use the pull start (see above, I have no choice) as that electronic start sucks. most times it doesn't even try to turn over.
So fingers crossed replacing it will solve the issue. Closest dealer is 50kms away, Generac won't send me the switch to unplug and change a few wires. They suggested I see if the dealer will pickup/drop off at my expense of course instead of me making 2 100km round trips to drop off and pickup.
So the product to me is average.. I'd expect much more for the price of this item and better service from the manufacturer. Both are just average at best.
Date published: 2022-05-06
Rated 5 out of
5
by
Kevin from
Long Haul
Electric pressure washers usually last me 2years due to heavy use. Cars, motorcycles, UTV’s, ATV’s, and household chores. I have used this gas pressure washer, at least weekly, for the past 5years. Worth every penny of $399 years ago and it’s still the same price! The hose finally blew out 3 days ago and I’m here looking for a replacement and decided to go ahead and leave a review. I highly recommend Generac and this pressure washer!
Date published: 2022-04-30
Rated 5 out of
5
by
Hunter from
great features
Really like the electric start. Looks like a very good warranty.
Date published: 2022-04-21
OneWash Pressure Washer - 6602 is rated
4.6 out of
5 by
474.