Financing Options for Home Generators and Standby Power Solutions Financing Options for Home Generators and Standby Power Solutions

Financing plans for home generators

Take charge of the way you pay with great financing options from Generac and Synchrony.

Apply for financing today!

Protect your home and family with backup power options today and pay overtime with the Synchrony Project Card. Plus, receive these exclusive benefits:

  • Dedicated credit limit for your future home improvement projects
  • $0 fraud liability
  • Hassle-free application process with fast credit decisions
  • Promotional financing with convenient monthly payments

Feel the power of flexible financing with the Synchrony Project Card.

Get an Estimate

Apply for financing in three easy steps!

pin point icon

Find a local dealer
with "Financing" listed in their description.financing icon


question icon

Ask
about the financing options they offer.


paper icon

Apply
for financing.

9.99% APR with fixed monthly payments for 132 months with the Synchrony Project Card

Fixed monthly payments required equal to 1.25% of the highest balance applicable to this promo purchase until paid in full. $29 account activation fee will apply.

Image of a Generac home standby generator next to the siding of a house

Purchase a Generac unit with no interest if paid in full in 18 months with the Synchrony Project Card

Interest will be charged to your account from the purchase date if the promotional balance is not paid in full within 18 months. $29 account activation fee will

Learn How  

A homeowner and a dealer looking over a phone together next to a Generac home standby generator

 

Special Financing Options

Generac offers a variety of financing options for your home generator system purchase. Click the button below to find out more!

See if you Prequalify   Apply Now

with no impact to you credit score

blue background

For Current Cardholders

Need to pay a bill or update your account information? Login here or contact Synchrony Bank Customer Service at 1-866-396-8254.

FAQs About Home Generator Financing & Costs

We've got answers to some of the most common questions related to Generac home standby generator financing and costs.

The cost of a whole house generator depends on several factors, including the generator size, fuel type, installation requirements, and any additional accessories. Homes with higher electrical demands typically require larger standby generators, which can increase the overall investment. The best way to determine pricing is through a personalized quote based on your home's specific backup power needs. Installation is a separate cost and varies based on multiple factors.

Installation costs vary based on your property's layout, local permitting requirements, fuel source availability, and the complexity of the installation. Factors such as trenching, electrical upgrades, transfer switch installation, and site preparation can all impact the final cost. An in-home consultation provides the most accurate estimate for your specific project.

Yes. Many homeowners choose to finance a home standby generator to spread the cost over manageable monthly payments instead of paying the full amount upfront. Financing options may be available (such as competitive interest rates, extended repayment terms, and promotional offers) for both the generator equipment and installation costs, making it easier to invest in reliable backup power for your home. A financing specialist or authorized installer can help you explore options that fit your budget and household needs.

Yes. Like any other piece of equipment with an engine, a standby generator requires periodic maintenance to help ensure reliable operation. Ongoing costs may include routine service, replacement parts, fuel usage during outages, and optional monitoring or service plans. Regular maintenance can help maximize generator performance and extend the life of the system.

Available tax credits, rebates, and incentives vary by location and may change over time. Some homeowners may qualify for local utility incentives, emergency preparedness programs, or other regional benefits. Homeowners should consult with a tax professional, utility provider, or local authorities to determine what programs may apply in their area.

A home generator may increase your home's appeal, particularly in areas where outages, extreme weather, or aging electrical infrastructure are ongoing concerns. Some sources, including Consumer Reports, suggest this translates to a 3% to 5% increase in home value, though that figure should be understood as a potential range rather than a guaranteed return.

Generac does not currently offer a direct, corporate-wide trade-in program for home standby generators. However, many independent Generac installers offer local buy-back or trade-in programs when you upgrade to a new whole-home system. The trade-in works similarly to a car trade-in, where your existing unit is evaluated and that value is then deducted from the replacement purchase or installation cost. We recommend asking your area's certified installer to see what your options are.