*Liberty Utilities Special Offer Terms and Conditions
Offer redeemable only when customer schedules a free in-home assessment with Generac Power Systems’ Consumer Sales Team (not directly with the Generac dealer). Customer must also purchase a new and qualifying Generac automatic standby generator with a participating authorized Generac dealer*. Refurbished products are excluded from this offer. The free promotional items are: a 7-year extended-limited warranty for air-cooled and liquid-cooled home standby generators, first year of maintenance and one year of dealer monitoring. Generac Power Systems provides the 7-year extended limited warranty, while the first year of maintenance, first year of dealer monitoring is provided by the Generac dealer that sold and installed the unit (must be one in the same). “Service” is defined as a one-time provision and installation of an inspection of fuel connections and battery terminals and the replacement of the oil, oil filter, air filter and spark plugs. Generator must be installed and activated in order for the warranty to be applied. The only Generac home standby generators that qualify for this promotion are the following models: 7031, 7032, 7033, 7035, 7036, 7037, 7038, 7039, 7042, 7043, 7141, and 7142. Limit one promotional offer per household. Proof of purchase along with other documentation may be required to receive this offer. Individual prices may vary. Generac reserves the right to modify and/or rescind this offer at any time without notice. Offer valid only on qualifying purchases made in the United States (excluding American Samoa, Guam, Northern Mariana Islands, Puerto Rico and the U.S. Virgin Islands).
Additional terms and conditions may apply. For more details, contact Generac Power Systems’ Consumer Sales Team at 844-848-6850.
*A participating authorized Generac dealer is a member of Generac Power System’s PowerPlay Team. All in-home assessments must be scheduled through Generac’s Consumer Sales Team, and all purchases must be made through a PowerPlay Team member to qualify for the promotion.