Emergency Preparedness

Three-Step Hurricane Preparedness Checklist: Protect Your Home & Power | Generac

4 MIN READ

   

Hurricanes and intense storms can hit when you least expect it. That’s why it’s so important to stay prepared, even when the forecast predicts sunny skies. A few simple steps now can help you avoid property damage, lessen strain on emergency services, and even save lives down the road. By getting ready ahead of time, you’re not just protecting yourself, you’re preserving your peace of mind.

A white house surrounded by trees and a pond, used to illustrate a home at risk in a hurricane-prone area

Step 1: Hurricane-proof your home

  • Unplug all non-essential electronics: Unexpected power surges can damage anything plugged into the wall.
  • Install surge protectors: They’ll safeguard sensitive electronics and appliances when lightning strikes.
  • Familiarize yourself with your breaker: If floodwaters make it into your home, your electrical system could become a hazard—make sure you know how to turn it off.
  • Secure windows with plywood: Boarding up windows can protect them from flying debris and keep water out of your home.
  • Protect against flooding: Line your foundation with sandbags to keep water from seeping in.
  • Trim your trees and greenery: Get rid of any weak branches that might break off in high winds.
  • Stock up on supplies: Keep a first aid kit, non-perishable food and drinking water on hand—enough to last you several days.

Try this hurricane preparedness guide for a detailed walkthrough on how to secure your home.

Generac home standby generator installed outside a house, shown as part of hurricane preparedness guidance

Step 2: Make sure your home standby generator is up to the task

If you have a backup generator, it’ll help you stay comfortable and connected when the power goes out. It can be your lifeline during a hurricane—but only if it’s prepared for the long haul.

Use this short checklist before storm season soyour generator isready to perform when you need it most.

  • Clean inside and around your unit: Removing obstructions will improve airflow and reduce the risk of overheating.
  • Check fuel lines: Make sure there aren’t any leaks or blockages—you’ll want fuel to flow smoothly when needed.
  • Inspect oil and air filter levels: Refill and replace if necessary.
  • Check spark plugs and battery: The plugs should be clean and the battery charged for easy startup.
  • Do a test run: Then, you can be sure it’s ready to go.
  • Stay on top of annual maintenance: Regular upkeep will help keep your generator running smoothly year-round.

Don’t forget: As storm season approaches, you’ll want to stock up on fuel. It’s important that your generator starts with a full tank, and though fuel consumption varies by model, it’s never a bad idea to keep extra on hand. Wondering how much gas your generator uses? You can calculate approximately how much you’ll need here.

 

 

Step 3: Research evacuation routes and pack the essentials

In some situations, the safest option will be to leave your home. It’s a difficult choice, but as storms shift and grow in strength, staying might become risky. In some situations, you might even face evacuation orders, so solidifying your evacuation plan ahead of time can help you stay calm and on-task through the chaos.

Your plan should include an emergency go-bag with all the essentials: important documents, medications, extra clothing and more. Assume you won’t have internet access and include cash and printed maps. Take note of nearby shelters and likely evacuation routes if you can. You also can check for recommendations from your local government to avoid last-minute confusion or congestion. And if your home isn’t flooded before you leave, turn off your breaker and unplug appliances to reduce the risk of electrical hazards or

damage when the power comes back. Having a plan in place means you can act quickly and stay safe, no matter what the storm brings.

A brown emergency go-bag containing essential items to pack when evacuating before a hurricane

Related articles