Image of Poudre Falls river near Fort Collins Colorado Image of Poudre Falls river near Fort Collins Colorado

Case Study

Headwaters Center Off-Grid Microgrid

  • 1 MIN READ
  • Commercial Buildings

An Off-Grid Microgrid in Winter Park, Colorado

The Headwaters Center blends history with innovation—designed using materials from the past and powered by the energy systems of the future.

Constructed from a disassembled and relocated Civil War-era barn originally from Ohio, this unique facility in Winter Park, Colorado, is a model for sustainable development. The Headwaters Center is completely off-grid, operating independently from the electric utility thanks to a self-sufficient, off-grid microgrid system.

The facility derives most of its power from the sun through an onsite solar powered microgrid, storing energy in a 300 kWh battery system. Much of the building’s load—including HVAC and air handling systems—is powered directly from the DC bus. AC loads are supported by Princeton Power’s grid-forming inverters, and the system uses backup natural gas generators only when necessary.

At the core of the energy infrastructure is the Generac Link microgrid control system, which acts as the primary user interface and control hub. This advanced microgrid technology delivers real-time performance monitoring, intelligent load management, and seamless coordination of solar, storage, and generator assets—enabling the site to operate in a generator-off mode as conditions allow.

By combining reclaimed architectural materials with cutting-edge microgrid software and controls, the Headwaters Center stands as a beacon of energy independence, environmental stewardship, and design innovation.

Energy Resource Capacity

  • 90 kW

  • 250 kW

  • 300 kWh

Headwaters Center

Princeton Power GTIB-480-125 Inverter (2)
125 kW
Toshiba LTO Battery (7)
172 kW/43 kWh
   
SMA CORE1 PV Inverters (2)
50 kW
DEIF AGC150 Natural Gas Generator (w)
100 kW
   
AccuEnergy AcuDC Meter (3)
RainWise PVmet 200 Weather Station (1)