Generac recommends having your unit serviced every 6 months by an IASD. To locate your nearest dealer, visit www.generac.com/dealer-locator.
Current owners of Generac air-cooled home standby generators greater than 13kW that were manufactured between 2008 and 2015 are eligible for a one-time, no cost inspection to determine whether the unit’s plenum (a component of the fuel system) has excessive corrosion due to poor installation or maintenance conditions. Current owners of systems meeting the above description can call 1-855-388-3181 or any authorized local service dealer for more details about receiving a free inspection. Please have your generator serial number and the address the generator is located at available when calling.
Owners of systems who either: (1) previously participated in the limited inspection program and incurred an $80 inspection fee; or (2) declined to have an inspection done at that time, have been sent a notice on how to submit a claim for a free inspection or for reimbursement of the $80 inspection fee they paid for the reduced cost inspection. Please refer to the notice provided for further instructions.
Keeping up with scheduled maintenance helps ensure your home standby generator operates in top condition and meets warranty requirements. Failing to perform scheduled maintenance can lead to your generator breaking down, just as a car might break down if oil is not changed or other maintenance intervals are missed. Scheduled maintenance helps protect your investment in your generator.
Maintenance requirements vary between home standby generator models, so always consult your owner’s manual for recommended maintenance intervals. Regular maintenance includes changing air filters, oil and oil filters, spark plugs, checking battery charge, sediment traps, valve clearance, inspecting the fuel system, and cleaning the generator from dirt and debris inside the enclosure and outside around the unit. The use of your generator determines maintenance intervals. Your generator will need oil replenished, fuel and oil line inspections, and inspection of enclosure louvers for dirt and debris if the unit is running daily, such as in a prolonged utility outage. Generac recommends contacting an Independent Authorized Service Dealer (IASD) to service your generator.
Generac recommends having your unit serviced every 6 months by an IASD. To locate your nearest dealer, visit www.generac.com/dealer-locator.